2026-03-17 11:27 PM - last edited on 2026-03-18 3:52 AM by Andrew Neil
Is this version do not copy touchgfx_core.a to project folder? ex) Middlewares\ST\touchgfx\lib\core\cortex_m4f\IAR8.x
because I did generate code in touchGFX so automatelly remove the files in lib/core.
and i can't build on IAR because .ipcf file generated from touchGFX desinger need touchgfx_core.a of path above.
2026-03-18 3:42 AM
Hello @daniel9.Which toolchain have you selected in STM32CubeMX?
Is the lib/core folder completely empty, or does it contain the library for a different compiler?
Can you share your project?
Best regards,
Johan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.