2025-03-03 9:18 PM
Hello All,
I am trying to use STM32H757I-Eval board for one of Development project and need to get one clarification regarding it.
I am using Touch GFX Designer Version- 4.24.2, while creating a new project I can see STM32H747l Eval for Board Setup in Touch GFX, but not STM32H757I-Eval.
Though I can run the sample code on STM32H757I-Eval using STM32H747l Eval base setup, Will this cause any major problem in my future development, or I can use STM32H747l for any STM32H7 Series Eval Board ?
BR
Solved! Go to Solution.
2025-03-03 11:23 PM
Hello,
STM32H757I-Eval and STM32H747l-Eval have the same hardware and the only difference between the two is that H757 has cryptography feature and H747 not. So you can use any of the board for TouchGFX.
Hope that answers your question.
2025-03-03 11:23 PM
Hello,
STM32H757I-Eval and STM32H747l-Eval have the same hardware and the only difference between the two is that H757 has cryptography feature and H747 not. So you can use any of the board for TouchGFX.
Hope that answers your question.
2025-03-09 9:28 PM
Hello @mƎALLEm
Thanks for the clarification.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.