2023-10-29 7:43 AM
Hello,
Could somebody explain what is the purpose of this second line of code below taken from main.c in TouchGFX example for STM32HB3I-DK?:
SDRAM_Initialization_Sequence(&hsdram1, &command);
*(__IO uint32_t*)(0xD0000000) = 0x11111122;
It works fine with provided example but my program (set up from scratch in CubeMX) is going to mem fault on this line. When I comment this line out my program works fine. D0000000 is start of address of external SDRAM. Is it something to do with testing speculative memory access? I know nothing about it.
Solved! Go to Solution.
2023-10-30 2:06 AM
Hello @RZasa.1 ,
Sorry for the inconvenience. Yes, the second line which is a write operation was meant for testing and should have been removed. So, you can easily ignore it.
Thank you for the notice
2023-10-30 2:06 AM
Hello @RZasa.1 ,
Sorry for the inconvenience. Yes, the second line which is a write operation was meant for testing and should have been removed. So, you can easily ignore it.
Thank you for the notice
2023-10-30 2:19 AM
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.