2022-07-15 6:57 PM
TouchGFX projects has a cube_programmer.mk in each project folder.
I have installed my CubeProgrammer in a different location to the default location in the cube_programmer.mk. I was wondering if the cube_programmer.mk is created on each project creation as part of the code within in the TouchGFX IDE or is it a file template which is copied from another location each time? I would like to change the master file so I do not have to change the project file each time.
2022-07-16 1:00 AM
Maybe simpler is use MKLINK and create symlink on default place
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.