2024-01-16 9:52 AM - edited 2024-01-16 4:48 PM
Hello,
I'm working on a vt100 terminal emulator, so I created a custom widget which decodes input stream and then display it on a TFT-LCD by LTDC. It works fine alone, after a custom keyboad added on the top, the simulation will crash when the custom widget try to draw the part under the keyboard, and visual studio throws an exception as shown in the screenshot.
what cause this result and how can I avoid it?
your help will be appraciated.
Solved! Go to Solution.
2024-01-26 3:28 AM
Hello @wonderFine ,
That's a pretty cool project you are working on :D
To be honest, it is very difficult to detect what is causing the issue, but a possible solution to hide the symptom would be to try auto scrolling the text to avoid cursor colliding with the keyboard.
Have you created the keyboard yourself?
2024-01-26 3:28 AM
Hello @wonderFine ,
That's a pretty cool project you are working on :D
To be honest, it is very difficult to detect what is causing the issue, but a possible solution to hide the symptom would be to try auto scrolling the text to avoid cursor colliding with the keyboard.
Have you created the keyboard yourself?
2024-01-27 3:32 AM
Hi, @Mohammad MORADI ESFAHANIASL
Thanks for your time.
The keyboard widget is ported from the Keyboard Example in touchGFX Designer.
It's strange that no error emerges when the cousor colliding with standard widgets (which provided by touchGFX Designer) :thinking_face:. Scrolling the text can avoid the symptom indeed. Thanks again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.