2020-07-23 4:25 AM
Hi,
I'm trying to create a touchGFX application for STM3F429I-DISC1 board in the custom board approach. I would like to adapt it later to a larger screen, that's why i want to configure it this way. So I have succesfully configured the FMC because after debugging my application, i can see that the frramebuffer (starting from 0xD0000000) is filled with (0xF800 - corresponding to the red color in RGB565 format), but nothing displays. The doubt remains on the ILI9341 initialization, even if I copied the same routines generated by TouchGFX for the stm32f429i-DIC1 board.
Do you have a idea about what could be the problem ?
Regards!
2020-08-17 2:37 AM
Hello,
What is your current status ?
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.