2020-06-22 7:50 PM
Thank you for helping.
STM32F746G DISCO with Application Template
Blank UI with UI Template
When you create it with this, the following display appears.
Creation of TouchGFX Application failed
What is the cause?
Is there a log to analyze the cause?
Thank you.
Solved! Go to Solution.
2020-06-23 4:24 PM
Hi Romain
After changing the AT compatibility, the error disappeared.
I was able to confirm the location of the log file.
Thank you very much.
2020-06-23 12:56 AM
Hi,
First: why did you chose to use 4.12.3 ? The latest version is 4.13 (with 4.14 coming soon) but is this a dev choice?
Could you provide more info/pictures on what you tried to do? You did not attach a picture like you meant to I suppose. I suspect you might be choosing an AT not compatible with an older version of Designer so that is why I would recommend trying 4.13 instead.
Otherwise you can go to %APPDATA%/TouchGFX-4.12.3/TouchGFXDesigner.log
/Romain
2020-06-23 3:15 AM
"Creation failed" could indicate that you cannot contact our package server to download the combination of AT and UI you've chosen. Check the logs in %APPDATA%/TouchGFX-4.12.3
2020-06-23 4:24 PM
Hi Romain
After changing the AT compatibility, the error disappeared.
I was able to confirm the location of the log file.
Thank you very much.
2020-06-23 4:24 PM
Hi Martin
Thank you for your reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.