2020-05-10 11:01 PM
Hi Team
I have LCD panel with 24-bit RGB Interface and having resolution of 800 x 480. I wanted to know about its support with part no. STM32L4S7VI as its having built-in TFT Controller. I know it has 24-bit RGB support, but does it supports 800 x 480 pixel resolution ?
2020-05-10 11:35 PM
Yes, but only with a reduced selection of colours, i.e. 256-colour palette mode.
The internal memory can't hold more than 1 byte/pixel at that resolution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.