2019-07-23 2:10 PM
Hello,
I am really new to the STM32 und TouchGFX World. So I bought a board STM32H747I-DISCO, the first thing I saw: not supported in STM32CubeIDE :(
I generated a new Project with TouchGFX, I selected the Application Template (16 Bit) with a Blank UI. I placed a Button With Labelk in the left upper corner:
- Generate Code: "Code generation complete"
- Run Target: "An error occured during flash. Please make sure you have the right target connected."
I used the STM32 ST-LINK Utility and downloaded the File "...\My Application\TouchGFX\build\bin\initflash.hex" - the result can be considered in the appendix :(
I am sad.
2019-07-25 11:22 PM
The GCC Makefile produces three target files after linking:
target.hex -> the entire application
intflash.hex -> application code and data placed in the internal flash of the MCU
extflash.bin -> binary data of all assets to be placed in the external flash
An elf loader is needed needed when an application contains code or data which is placed on a flash device outside the MCU.
/Anders
2020-11-02 5:57 PM
Hello,
Is it possible to just copy the hex file into its mass storage?
Or I really need to program it using STM32CubeProgrammer?
Is the STM32CubeProgrammer installed together with STM32CubeIDE? If so, its location?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.