2019-06-15 6:16 AM
Hi,
I am using DCMI peripheral on STM32H7 to capture an 320x240 monochrome image (1 byte per pixel) and DMA to transfer it to D1 SRAM. DMA uses FIFO, Threshold: Full, Data width: Word for both source and destination.
I would like to make a copy of that image array so I can analyse it while the original array is filling in with a new frame. I have done this using another DMA Memory-to-memory and it works great.
The problem is I have to manually start the DMA Mem-to-mem transfer. So I was thinking of using MDMA which can be hardware triggered by DCMI DMA.
I have spent whole day of trying to get MDMA working in that way, but I always get unsatisfactory results, i.e. sometime only cca. 50 image rows of 240 total are copied to the new array and sometimes none are copied. I tried to configure MDMA using CubeMX and change settings like:
Triger mode: Buffer transfer, block transfer, Repeat block transfer and Full transfer.
List type: Linear, Circular and Buffer Length.
I also tried changing arguments BlockDataLength and BlockCount when calling:
HAL_MDMA_Start (MDMA_HandleTypeDef *hmdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t BlockDataLength, uint32_t BlockCount)
But I never seems to be able to copy the whole aray (76800B). I have read AN for MDMA but still some things are foggy. Could somebody help me on how to configure the MDMA settings for this case?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.