STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Will ‘AppWizard’, currently being developed by SEGGER, be available in a future release of STM32Cube_FW_F7? Is there any indication as to when SEGGER will release ‘AppWizard’?

SEGGER who provides the emWin graphics stack is developing a new GUI Builder call ‘AppWizard’.  SEGGER have released preliminary previews of this new software tool on their blog here and here. 

Resolved! Chineese and corean only shows ???

I need some text in chineese and corean, for example i need to write 한국어 and 汉语 , i've added those letters in my Typographies, but still get only ???, what am i missing? another strange think is that i forgot to put greek character in my typography, ...

Zui by Senior
  • 4446 Views
  • 13 replies
  • 0 kudos

touchGFX and snprintf function

Hello,i use snprintf function to print some UnicodeChar variable. But i have trouble to get special charcters printed (as é, è, ü...) by the mean of this function.(even if i have declared in the typography wildcard Character column the special charac...

Getting somtimes Hardfault in GuiExec()

I was design a custom board with a MCU STM32F767BI, a LCD with 800x600 pixels and a SDRAM with 64Mb. I'm getting a HardFaultHandler after run some time the aplication and it faults inside the process GUI_Exec() according to the PC register. Analizing...

Nickjmas by Associate III
  • 1176 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.0.1 and TouchGFX

Hi there. Do you guys know by any chance if TouchGFX-related code generation issues have been resolved in the new version of STM32CubeIDE (v. 1.0.1)? Is it worth/safe to upgrade?

VK by Associate
  • 1006 Views
  • 1 replies
  • 1 kudos

STM32H7 - MDMA with DCMI

Hi, I am using DCMI peripheral on STM32H7 to capture an 320x240 monochrome image (1 byte per pixel) and DMA to transfer it to D1 SRAM. DMA uses FIFO, Threshold: Full, Data width: Word for both source and destination.I would like to make a copy of tha...

msiadj21 by Associate
  • 949 Views
  • 0 replies
  • 0 kudos

Resolved! Using Visual Studio for hardware integration?

Hello,is it possible to use VS for coding the hardware integration side of a TGFX-Application?I tried the following:I downloaded the example project from here.When I tried to make some modifications to model.cpp the Intellisense didn't find any comma...

CKauf by Associate III
  • 2855 Views
  • 5 replies
  • 0 kudos

Managing a rotary encoder.

Hi all,I'm using touchgfx with stm32f769 in a board with hardware buttons and hardware knob (rotary encoder). I have more screens and the knob is used to change values that are different for every screen. Is there an example on how I can implement in...

SCass by Associate
  • 1670 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.