2019-09-27 12:29 AM
Hi,
Having tested all the examples from the STM32F7 package for the STM32F769 Discovery kit, I started to write my own project from scratch. For thios, the starting point is the STMCubeMX tool.
So far, everything went well till I reached the point of the LCD. I cannot get it working. I compared the generated code with the one of the BSP. It is similar except in
Has anyone any experience and advices to get a LCD working from a STMCubeMX project ?
Thanks in advance.
Regards.
Solved! Go to Solution.
2019-10-01 11:08 PM
STMCubeMX has been having some problems with CubeIDE I believe they haven't fixed it. Personally I am following this method of sticking with TouchGFX and editing it through that. That seems to be working the best: https://www.youtube.com/watch?v=jQO7zhX0e0Q
You do run into the issue of not being able to then use CubeMX
If you don't care so much about the graphical libraries I would find the hello world example problem and maybe base your design on that?
2019-09-27 12:38 AM
2019-10-01 11:08 PM
STMCubeMX has been having some problems with CubeIDE I believe they haven't fixed it. Personally I am following this method of sticking with TouchGFX and editing it through that. That seems to be working the best: https://www.youtube.com/watch?v=jQO7zhX0e0Q
You do run into the issue of not being able to then use CubeMX
If you don't care so much about the graphical libraries I would find the hello world example problem and maybe base your design on that?
2019-10-09 11:47 PM
@TheCarterII Many thanks.
Indeed the STM32CubeMX project is generated. But when generating the project, I can also notice that TouchGFX also added some tweaks in the generated code.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.