2021-08-24 12:06 AM
Hi,
I have been using STM32F746 with TFT's of Medium Sizes up to 4.3" having RGB Interface on my custom boards. Now I want to Interface Large Display like 12.1" or 15". I know I need a RGB -LVDS Converter Chip , But I want to know How to use LTDC with LVDS Display Datasheet. Attached is a datasheet of Winstar 12.1" Display Module. I'm not able to understand the horizontal & vertical back, front porch values from the datasheet.
kindly help me with this.
2021-08-24 2:55 AM
Hello @SMour.2 ,
I recommend you to have a look to Application note AN4861 available on our Website
This application note describes the LCD-TFT display controller of the STM32 and demonstrates how to use and configure the LTDC peripheral.
Imen
2021-08-24 3:49 AM
Hi Imen,
I'm aware of LTDC and have been using it with RGB interface Displays. I want to know how to use LVDS Display which is operated only in DE Mode and HSYNC VSYNC input signals can be set to Low Levels. Does That Mean I don't need Horizontal & Vertical back, front porch values and can set them to 0? The Display datasheet says "Since this assembly is operated in DE only mode, Hsync and Vsync input signals should be set to low logic level. Otherwise, this assembly would operate abnormally."
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.