2020-04-05 5:11 PM
hello
i am designing a custom board and i need to interface a PI camera with MIPI-DSI interface.
i need to know if the video data provided by the PI-camera is handled by the STM32F479VI MIPI-DSI interface.
regards.
Zakaria
2023-03-29 2:41 AM
MIPI-DSI is for the display interface, can't be used in the camera part. the camera is using the MIPI-CSI interface, now ST MP1 is supporting the interface.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.