2016-07-12 4:08 PM
Hello everyone,
I want to use a 1280x120 display (16bit parallel RGB interface) with a STM32F469.The datasheet says that it can only support a maximum resolution of 1024x768.The horizontal resolution of my display is a bit higher, but my total bandwith schould be much less, because the vertical resolution is so low.Is it possible somehow?Thanks for your help,Moritz #stm32 #lcd #tft #stm32f4692016-07-12 5:35 PM
Is it possible somehow?
Probably, its a matter of total memory size, bandwidth, and width of control registers. If you don't violate the first two, it will come down to the last. Make sure there is a >10-bit register describing the width of the screen raster.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.