2020-02-05 7:18 AM
Has anyone been able to create a working project with CubeMX 5.5 and TouchGFX 4.13?
Solved! Go to Solution.
2020-03-31 8:16 AM
Did you check the Application template from the designer?
There's a new version 3 up that supports CubeMX 5.5!
/Martin
2020-03-31 8:16 AM
Did you check the Application template from the designer?
There's a new version 3 up that supports CubeMX 5.5!
/Martin
2020-03-31 10:08 PM
I did at first, but it wasn't there. Now I see that there is a new template version there. Thanks for posting this, and I will give it a try.
Matej
2020-04-15 11:18 AM
I have tried it out and if you are using the template screen transitions are not working on device (project built with cube IDE), but are working fine in the TouchGFX Simulator. Is there something that needs to be enabled?
Thx Matej
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.