2018-02-15 7:44 AM
Hello All
My Requirement as Below:Connect OV7670 Camera Module (Or Any Other Module with Support 640x480) with STM32F407VGT6(100Pins) and Get 640x480 Grayscale Image at Minimum 7 FPS Directly on Windows PC Through USB & Android Through OTGAs Per My Research i Found Below Things:
- I Can Use DCMI To Connect Camera with STM32F407VGT6. Also i Have Some Example Of It.But Where i Stuck is - How to Transfer That Data To PC & Android Over USB? (Because in All Example There is USB To UART Used)- Which Interface Need Full Speed OR High Speed?Also I Want To Transfer That Data in Bulk Transfer Mode to PC
- as Per My Knowledge Libusb Makes My Task Easy on PC & Android, But Confusion is How to Write Driver For MCU?- I See Example of HID, Custom HID, CDC But i Have Not Seen Any Example of Vendor Specific Class Driver For ST MCU- Is It Possilble to Modify HID,Custom HID, CDC Driver To Satisfy My Requirement?
Lets Clear Also Some Things:- I dont want to store any image on board if its not require compulsory- I dont want to do any image processing onboard if its not require compulsory- I Just want 7 FPS of Camera 640x480 Resolution Grayscale - All Image Processing i doing through software on windows & app on android.- I Only Need Direct USB Connection, I DONT WANT USB TO SERIAL CONNECTION - I WANT PURE USB CONNECTION- I Dont want to Implement UVC Drivers, I Need Bulk Transfer.- Please Dont Suggest Wi-fi, Bluetooth or Anyother Communication Because I Need Only Through USBI am Programming Guy very familiar with C♯, C++, .Net, Eclipse, Android, Java, PHP.
But im New to STM32F4 But I have done Basic Projects with That to Understand how its works and i also successful in that.-Thanks in Advance.
#vendor-class-driver #stm32f4 #otg #dcmi #vendor-specific-driver-usbWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.