2022-10-23 6:25 AM
Hello,
I've found a bug during code generation using STM32CubeMX on STM32H725AE MCU.
STM32CubeMX doesn't generete correct code for DMA2D using RGB565 format.
In function:
void MX_DMA2D_Init(void)
{
/* USER CODE BEGIN DMA2D_Init 0 */
/* USER CODE END DMA2D_Init 0 */
/* USER CODE BEGIN DMA2D_Init 1 */
/* USER CODE END DMA2D_Init 1 */
hdma2d.Instance = DMA2D;
hdma2d.Init.Mode = DMA2D_M2M;
hdma2d.Init.ColorMode = DMA2D_OUTPUT_RGB565;
hdma2d.Init.OutputOffset = 0;
hdma2d.LayerCfg[1].InputOffset = 0;
hdma2d.LayerCfg[1].InputColorMode = DMA2D_INPUT_RGB565;
hdma2d.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
hdma2d.LayerCfg[1].InputAlpha = 0;
hdma2d.LayerCfg[1].AlphaInverted = DMA2D_REGULAR_ALPHA;
hdma2d.LayerCfg[1].RedBlueSwap = DMA2D_RB_REGULAR;
hdma2d.LayerCfg[1].ChromaSubSampling = DMA2D_NO_CSS;
if (HAL_DMA2D_Init(&hdma2d) != HAL_OK)
{
Error_Handler();
}
if (HAL_DMA2D_ConfigLayer(&hdma2d, 1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DMA2D_Init 2 */
/* USER CODE END DMA2D_Init 2 */
}It doesn't generate this line, which causes wrong pixel color to be displayed.
hdma2d.Init.BytesSwap = DMA2D_BYTES_SWAP;BR,
JN
2022-11-02 1:41 AM
Hello,
First of all let me thank you for posting.
Could you please provide the *.ioc file and the CubeMx and CubeIDE version so I be able to investigate the issue.
Kind regards,
Aymen
2022-11-03 11:44 AM
Hello,
Thank you for the respond. I'm sorry, but i cannot provide *.ioc file, because the project is private. The version of CubeMX is 6.6.1. I'm not using CubeIDE, just CubeMX. I hope it will be helpfull.
BR,
Jan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.