2019-12-15 6:51 PM
2019-12-16 4:09 AM
Please be more specific. Are you talking about a specific demo or example in the Cube FW packs?
/Martin
2019-12-16 7:08 AM
Hi Martin,
2019-12-16 7:09 AM
STM32Cube_FW_L4_V1.14.0\Projects\32L4R9IDISCOVERY\Demonstrations\TouchGFX without source code.
2019-12-16 7:11 AM
if using TouchGFX 4.12.3 Designer to generate the "TouchGFX Watch" project for 32L4R9IDISCOVERY, it has IAR and gcc only, is there any Keil project ?
2019-12-16 7:12 AM
More, any Good TouchGFX tutorial for helping us to change the LCD of 32L4R9IDISCOVERY to customer's one ?
2019-12-17 1:29 AM
"TouchGFX Watch" can be run up on EVB 32L4R9IDISCOVERY, thank you.
2019-12-17 1:30 AM
Here comes next question, how to modify it to use customer's 454x454 MIPI LCD ? any application note ? thank you !
2019-12-17 1:34 AM
No Keil project, but you could probably make it yourself.
2019-12-17 1:35 AM
I'll check if this is something i can share.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.