2025-12-15 3:51 PM
Hi all
I have STM32 IDE installed in "C:\STM\STM32CubeIDE_1.19.0\STM32CubeIDE" and seem to work properly so far as I am on installing the 2 programs.
I try to install TouchGFX 4.26.0 in "C:\STM\ to have those two in the same area., but I received an error
like this one: Could not set file security for file "C:\STM". ERROR 5.........
So anyone have an idea ?
Thanks all.
Solved! Go to Solution.
2026-01-06 2:27 AM
Hello @Dany0 ,
I've not seen this issue before. Do you confirm you can install and run TouchGFX when it's located somewhere else from the STM3CubeIDE folder?
2026-01-06 2:27 AM
Hello @Dany0 ,
I've not seen this issue before. Do you confirm you can install and run TouchGFX when it's located somewhere else from the STM3CubeIDE folder?
2026-01-26 4:49 AM
Hello @Dany0 ,
Do you have the answer to my pervious message? It will help me to figure out where the issue is :)
@Osman SOYKURT wrote:
Hello @Dany0 ,
I've not seen this issue before. Do you confirm you can install and run TouchGFX when it's located somewhere else from the STM3CubeIDE folder?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.