2021-04-17 9:44 PM
Hello there, I am actually new in coding STM32 boards. I am currently working on an STM32 F746G-DISCO.
i am using the "LCD_UsrLog ((char *)" to print messages on the LCD tft screen.
I am wondering if there some high level function that enables me to clear the messages I show (only messages and not the totality of the screen.
Thank you in advance
Solved! Go to Solution.
2021-04-19 2:43 AM
Hello @WBen .2 and welcome to the STM32 Community =)
Clear the whole LCD using BSP_LCD_Clear() function or only one specified string line using the BSP_LCD_ClearStringLine() function.
Have a look at this example available under STM32CubeF7 which can be a starting point for your project:
STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Examples\LTDC
May this application note helps you:
Please mark my answer as best by clicking on the "Select as Best" button if it helped:smiling_face_with_smiling_eyes:
Imen
2021-04-19 2:43 AM
Hello @WBen .2 and welcome to the STM32 Community =)
Clear the whole LCD using BSP_LCD_Clear() function or only one specified string line using the BSP_LCD_ClearStringLine() function.
Have a look at this example available under STM32CubeF7 which can be a starting point for your project:
STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Examples\LTDC
May this application note helps you:
Please mark my answer as best by clicking on the "Select as Best" button if it helped:smiling_face_with_smiling_eyes:
Imen
2021-04-20 8:20 PM
Thank you so much Imen, this was definitely helpful :thumbs_up::thumbs_up:
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.