2020-05-31 2:12 AM
Hello,
I have made an STemWin example with STM32F407 and ILI9341 with SPI interface.
I think that there is an graphic driver problem. The graphics are not sharp. What Could be the correct driver settings ?
My settings are;
pDevice = GUI_DEVICE_CreateAndLink(GUIDRV_FLEXCOLOR, GUICC_565, 0, 0);
GUIDRV_FlexColor_SetFunc(pDevice, &PortAPI, GUIDRV_FLEXCOLOR_F66709, GUIDRV_FLEXCOLOR_M16C0B8);
Solved! Go to Solution.
2021-03-29 5:06 AM
I resolved my issue by using the code line below
pDevice = GUI_DEVICE_CreateAndLink(GUIDRV_FLEXCOLOR, GUICC_M565, 0, 0);
2020-05-31 2:22 AM
Looks more like power supply problem.
JW
2020-05-31 2:27 AM
I am supplying the LCD via 5V. There is no problem with the supply.
2021-03-29 5:06 AM
I resolved my issue by using the code line below
pDevice = GUI_DEVICE_CreateAndLink(GUIDRV_FLEXCOLOR, GUICC_M565, 0, 0);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.