2020-04-22 7:16 AM
Hi,
Is there a way to compile the firmware using GCC in different computers or in a faster server available in local network?
I am using STM32CubeIDE, GCC, TouchGFX and my compile time is increasing as the code sizes increases too. Now I take about 5 minutes to compile...
I've found some applications to build a "farm of compilation", along different computers in local network, but it was for Linux, I'm Windows user.
*I have already tick "Enable parallel build" in C/C++ Build.
Regards,
Anderson
2020-04-22 7:20 AM
5 Minutes seems like a very long time. I'm assuming you have a fairly new computer.
Something like antivirus interrupting?
/Martin
2020-04-22 7:37 AM
Hi @Martin KJELDSEN
Thanks for reply.
It takes 5 minutes when I do Clean>Rebuild All. When I only Build it takes about 2 minutes... but still long time.
No, I've tested without antivirus working and my computer is a good one.
I've tested in others computers and I get the same result with this code.
Some time ago I tried the new version of Touchgfx in H7, and it took about 20 seconds to compile, very fast. Of course there was one screen and no long code. I don't know if the version can affect compile time...
I have 13 screens and my firmware takes about 5MB of flash.
Anderson
2020-04-22 7:40 AM
Peculiar. You could send the project to me and i could try it.
2020-04-22 7:54 AM
Sorry, but it is code from my company, I can't share.
But if there is some test that I can do here please let me know.
What I could see in Compile Console is the Touchgx files, I think 80% of time is spent on this...
What time would be expect in a code with this size for example? Is too away from mine?
2020-04-22 12:54 PM
in my case it helped a lot to switch off the *.bin file generation...
project -> properties -> c/c++ build -> Settings -> mcu post build ouputs -> tool settings tab -> uncheck "convert to binary file"
these bins can get really large and depending on your storage place (network share ?) this can cause some trouble.
2020-04-22 7:00 PM
I know someone who uses ccache with Atollic. Should work for CubeIDE too.
On Windows, you can use Linux tools in a container or VM.
The initial step of "headless" scripts (initialization of workspace, importing the projects into workspace) takes quite long time, even before compilation starts. if ST developers could improve *this*, would be super great.
-- pa
2020-04-22 7:16 PM
But for Eclipse CDT generally, go to Settings, C/C++ Build, Behavior tab, enable Parallel build.
2020-04-23 3:32 AM
Thanks for answer, but I've already unchecked this option
I have enabled only hex file..
2020-04-28 7:16 AM
This one I've already enabled..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.