2024-08-24 3:22 AM
hi
I have a problem, when I launch the simulator it does not launch the right project. My project is GP_Dash_70_V1_a not MyApplication_10.
MyApplication_10 is a project that I deleted a long time ago.
I do not know what manipulation I could have done to have this problem!
2024-08-26 1:10 AM
up please
2024-08-26 2:55 AM
Hello @NicoEFI ,
Did you rename your project after you created it?
Does it happen with all new projects that you create?
2024-08-26 3:17 AM
Hello @Osman SOYKURT I had to copy and rename it a long time ago, and the renamed project worked fine. Due to errors I had to reopen the old base project in the project that worked and the problems started. I think it was stm32cubeide that merged!
No problem with the new project.
Is there a file that contains the links to the files to open on the simulator? I haven't tested on the riverdi screen.
2024-08-29 7:14 AM
Hello @NicoEFI,
You can delete the generated, config, build, and simulator folders from your TouchGFX project directory, and regenerate the code from TouchGFX designer. Maybe this will help you, and please have a backup of your project before applying these changes.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.