2022-07-26 8:18 AM
Hi There,
I have a unusual question. We would like to use TouchGFX to design a simple GUI for a Yocto SOM Board an tried to cross compile a trial project. Compiling fails at linking because the touchgfx library libtouchgfx.a is not compatible.
So my question is. Has anyone tried something like this? Is it not recommended because of some reasons?
Kind Regards
Lukas
2022-07-26 10:49 AM
Designer not work under linux then for what simulator? Why not direct debug onboard?
2022-07-26 10:49 PM
What do you mean with debug onboard? The generated designer code compiles and runs perfectly under linux: Prerequisites | TouchGFX Documentation.
The problem is that I cannot cross compile it for Yocto, so I cannot debug or run the code on the SOM board. @TouchGFX Team did you ever do something like this?
2022-07-26 11:41 PM
2022-07-27 8:22 AM
Thanks for the quick answer. I did check the library and got the same output as you. I do take this library but when I compile with:
x86_64-fslcsdk-linux/usr/bin/aarch64-fslc-linux/aarch64-fslc-linux-g++
I get these linking errors:
.../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/9.3.0/real-ld: cannot find -ltouchgfx
../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/9.3.0/real-ld: cannot find -lSDL2
../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/9.3.0/real-ld: cannot find -lSDL2_image
../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/9.3.0/real-ld: skipping incompatible touchgfx/3rdparty/libjpeg/lib/linux/libjpeg.a when searching for -ljpegI dont get why it should not be compatible. Any ideas?
2022-07-27 9:11 AM
first 3 is about bad path to library search
last skipp is for libjpeg.a why mut check yuo
2022-07-27 11:25 PM
You are right, but I forgot to post the most important warning:
../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/9.3.0/real-ld: skipping incompatible touchgfx/lib/linux/libtouchgfx.a when searching for -ltouchgfxThis is not because of wrong path, it skipps the library because of compatibility. Do you have any idea if this can be fixed?
If I compare the readelf of a successfully compiled program for yocto I see one diffecence to the touchgfx:
Class: ELF64
Data: 2's complement, little endian
Version: 1 (current)
OS/ABI: UNIX - System V
ABI Version: 0
Type: DYN (Shared object file)
Machine: AArch64
Version: 0x1
Entry point address: 0x9a0The Machine Type is AArch64. Does that cause the incompatibility?
2022-07-28 12:24 AM
2022-07-28 1:49 AM
Yes I need the touchgfx library for AARCH64. Is it possible to get this from @Touchgfx Team?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.