2020-10-15 2:01 AM
Hey,
i am planning to use an LCD With RGB 18 bit interface.
In the LCD D.S there are only RGB+DE+DCLK Pins, without Hsync and Vsync.
it works In DE mode without this pins.
can the MCU work at this mode?
Br
peleg
2020-10-15 2:18 PM
Which mcu?
But, as all LTDC signals are outputs, whichever the mcu is, it really does not care whether that output is connected anywhere or not.
JW
2020-10-15 2:54 PM
Hey,
STM32H743..
Maybe there is a configuration register where you decide in which mode to work with.. H+Vsync or DE only.
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.