2025-06-25 5:26 AM
Hello
I have a lot of assets, both images and texts, that I need to use across multiple projects. Is it possible to link to the assets without creating a local copy in the project?
When I add an image in the designer it copies from the original location to the project assets\images folder. Can I not just set a relative link from the project folder to the folder that holds the assets?
Thank you in advance.
2025-06-25 5:49 AM - edited 2025-06-25 5:50 AM
Hello @Aagaard and welcome to the ST community,
In the TouchGFX designer, simply browse to the folder where the images are located in your local disc:
1- Select the image option
2- Click on "Project"
3- Click on "+" behind "images". You will prompted to the explorer.
2025-06-25 5:54 AM
I know how to add images to the project. This creates a local copy, just like going into images and importing.
I want to add a path to the image without generating the local copy.
2025-06-25 5:55 AM
If I remember correctly, there are general Eclipse methods to achieve such shared ("linked") resources.
Although this has always been one of the most awkward and anti-intuitive topics with Eclipse ...
2025-06-25 6:06 AM - edited 2025-06-26 12:31 AM
Hello @Aagaard,
There's no way to do it out of the box, you can also do some versioning git.
Br,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.