2020-06-19 11:05 AM
Hi to all!
I trying to run my first application of TouchGFX on custom hardware and I have some difficulties to integrate my code with the TouchGFX.
At the moments. i can't use my I2C touchscreen driver. I have tested it in a test project and in this project, I able to read the touchscreen coordinate, but if I use the same code in the TouchGFX project, I can't read nothing. After start a I2C read, I receive a stop condition and a nack..
How I solve this problem?
Another problem that I have encourred is that the signal events API of the RTOS don't work as expected, I have solved this using queue, but i'm not very happy ..
Someone can give some help?
2020-06-19 2:33 PM
I have found the problem.. It was a my mistake! By default the IC21 peripherical use the pins PB6 and PB7 but in my setup I use the pin PB8 and PB9...
Now i try to find why the signal events on one project works and on another project don't works..
2020-06-21 7:52 AM
Now the signal events work, but I don't understand why! I have done only the I2c pins change..
Maybe one day i will understand.. :)
2020-06-21 4:57 PM
I don't really have enough information to give you any real insights here :) Glad you solved the immediate issue though.
2020-06-22 12:57 AM
Maybe is my fault, I don't know. Some weeks ago, I had the same problem with another RTOS project and after a few days i have solved, but i don't know why..
Keep in mind that i haven't so much experience in RTOS and STM32 enviroments, so is very likely that I have done some errors somewhere.. :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.