2023-05-01 5:50 AM
Hello!
The CircleProgress and Circle widgets do not work with images on STM32H7 with a 1280x800 24bpp TFT (double buffered graphic mode), while they work correctly in the simulator.
Circle widget:
if under "Image & Color" I choose Color, it works on both hw and simulator but if I choose Image and assign an image, it doesn't work on hw but on the simulator it does.
CircleProgress widget:
if I select color, it works on both hw and simulator.
if I select an image for the background, it works both on hw and simulator.
but if I also select an image for the foreground progress, on the simulator it works while on the hw I only see the background image.
All other widgets and texts are rendered fine.
png images are both 348x348 32bpp, fully opaque (no trasparency), no matter if they are filled with a single color or not.
Circle center position at 174,174, radius 174, line Width 0 or 90 (probably won't work at any width), start angle any, end angle 360, cap style flat, alpha 255.
Please help.
Stefano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.