2021-03-24 2:05 PM
2021-03-24 6:06 PM
Hello Sozde.1,
Do you have the same issue on the simulator ? Also can you try see what is invalidated when running the simulator ? (press F2 when the simulator is running)
F429 is not powerful enough to be used efficiently with huge display like 1024x600. I don't know if it could have an impact in your case but it's important to take that into account.
Your display is an LTDC display ? Please provide more information about your current setup (software versions, board, external flash, external ram, etc.)
/Alexandre
2021-03-24 11:36 PM
Dear Alexandre,
simulator works normally.
I did not observe any changes with the F2 key.
We use our own coreboard.
CPU STM32F429IET
SRAM IS42S16400J-7TLI
FHASH M29W256GL70N6
TFT NHD-10.1-1024600AF-ASXV#-CTP-ND 10.1" TFT w/CAPTOUCH
We used it on a 7 inch screen (800x480) before. there was no problem.
We are currently planning to test with STM32F746IET.
we couldn't understand my hardware or software problem!
What do you recommend. thanks.
2021-03-24 11:40 PM
Keil v5.29 (ARM Compiler v5.06 update 6 (build750)
TouchGFX Designer 4.15.0
2021-03-28 11:34 PM
Hello Soner,
Did you check your clocks ? What's your display clock speed ? Are your framebuffers in external SRAM ? What's the bandwidth of this SRAM ? Same for Flash.
I suspect your clock frequencies are two low and the bandwidth is limited.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.