2021-03-27 9:51 AM
Hi
I start with a template. I'm generating GFX without error. I open the STM32CubeIDE. There are * .cpp files. There is no * .hpp. Why?
Regards
Andrzej
Solved! Go to Solution.
2021-03-28 11:41 PM
Hello,
This is how CubeIDE works. When you open the project in CubeIDE, the headers (.hpp) are at the top of the project but they are included. If you build the project it should work. FYI, to include other header files you need to go to the project properties and add includes paths.
So if I understand your question correctly, this is not a TouchGFX question but a question on how to use CubeIDE right ?
/Alexandre
2021-03-28 11:41 PM
Hello,
This is how CubeIDE works. When you open the project in CubeIDE, the headers (.hpp) are at the top of the project but they are included. If you build the project it should work. FYI, to include other header files you need to go to the project properties and add includes paths.
So if I understand your question correctly, this is not a TouchGFX question but a question on how to use CubeIDE right ?
/Alexandre
2021-03-29 12:31 AM
Hi
I start working with a template. Does the GFX template generate files to the IDE from * .hpp? Where does it need to be set?
Andrzej
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.