2021-10-09 2:58 AM
Hello,
I'm working with stm32h757i-eval board.
I have generated a code using the example code for keypad from touchGFX.
During the debug the below is the message i received.
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-Link Server is running on port : 7184
ST-LINK SN : 003600263137510F33333639
ST-LINK FW : V3J8M3
Board : STM32H757I-EVAL
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a00324.srec
File : ST-LINK_GDB_server_a00324.srec
Size : 377216 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:04.057
Verifying ...
Download verified successfully
But when I run my code There is nothing being shown on the display.
And after I run the code
These are the messages received.
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-Link Server is running on port : 7184
ST-LINK SN : 003600263137510F33333639
ST-LINK FW : V3J8M3
Board : STM32H757I-EVAL
Voltage : 3.27V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09984.srec
File : ST-LINK_GDB_server_a09984.srec
Size : 377216 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:04.066
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
But nothing is being displayed in the board.
I have attached the .ioc file for your reference
I have been working on this issue from a couple of days but there is no solution.
2021-10-09 4:17 AM
When you place breakpoint to main in both cortex for example to line gpio init , your code stop here or debuger lost connection soon?
As i write on other your Q better is start with example in TouchGFX without use IDE .
And too if you are beginner better is choice single core board.
2021-10-09 4:55 AM
Thank you for your response.
I started with the example code from the TouchGFX designer software and it has worked fine.
I want to customize my display configuration for which I have coded and has compiled successfully but I'm not able to display any content on the stm32h757i-eval board.
2021-10-09 4:59 AM
Sorry , but you need here write code and not what you do. We arnt Avengers...
2021-10-12 4:44 AM
Hi,
Were you able to write to your display before setting TouchGFX ?
If yes, can you check if the framebuffer is updated and sent to the display ?
/Romain
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.