2025-07-10 6:50 AM - edited 2025-07-11 8:51 AM
I have a custom board. Right now we have a "template project" which is mostly a stripped project and we have a customer project. We periodically merge some changes between them. Instead of copying the template project and modifying it I would like to be able to use it as a board in TouchGFX designer directly. This will be important when we will use the board for more than 1 customer.
I followed the instructions, but the board doesn't show up.
I followed these instructions: https://support.touchgfx.com/docs/development/scenarios/scenarios-create-at
I stripped the project.
My project structure is:
C:\source\company\company-stm32-touchgfx-hmi-bsp
C:\source\company\company-stm32-touchgfx-hmi-bsp\.git
C:\source\company\company-stm32-touchgfx-hmi-bsp\Doc
C:\source\company\company-stm32-touchgfx-hmi-bsp\Source\Middlewares
C:\source\company\company-stm32-touchgfx-hmi-bsp\Source\TouchGFX
C:\source\company\company-stm32-touchgfx-hmi-bsp\Source\TouchGFX\company-STM32-TouchGFX-HMI-BSP.touchgfx
I closed TouchGFX Designer
In TouchGFX environment terminal:
cd "C:\source\company\company-stm32-touchgfx-hmi-bsp"
/c/TouchGFX/4.25.0/designer/tgfx.exe pack -d Source
company-STM32-TouchGFX-HMI-BSP.zip is created
MyApplication.json is created
add some details to MyApplication.json
leave PathToDotTouchGFX empty as TouchGFX is in the root of the projectfolder
/c/TouchGFX/4.25.0/designer/tgfx.exe pack -rc -d Source
rename MyApplication-1.0.0.tpa to company-STM32-TouchGFX-HMI-BSP-1.0.0.tpa
moved company-STM32-TouchGFX-HMI-BSP-1.0.0.tpa to C:\TouchGFX\4.25.0\app\packages
Opening TouchGFX Designer doesn't show the board under partners.
Solved! Go to Solution.
2025-09-23 6:07 AM - edited 2025-09-26 6:02 AM
I was able to get it to work.
git clean -fdx (to remove build artifacts and other untracked files)
Open TouchGFX environment terminal
cd to parent directory
/c/TouchGFX/4.25.0/designer/tgfx.exe pack -d project_name
add some details to project_name.json:
"PathToDotTouchGFX": "TouchGFX",
"Type": "TGAT"
remove .git folder from zip and other files you want to remove (I remove some documentation)
/c/TouchGFX/4.25.0/designer/tgfx.exe pack -rc --version=1.1.1 -d project_name
copy tpa file to C:\TouchGFX\4.25.0\app\packages
Only issue I have now is that I'm trying to run some TouchGFX demo's and they are not all working:
2025-07-11 7:14 AM - edited 2025-07-11 7:47 AM
I discovered that adding or modifying boards in C:\Users\USERNAME\AppData\Roaming\TouchGFX-4.25.0\Downloads did work.
Instead of generating a .tpa file I tried to modify an existing one. Those files are just zip files renamed. I modified the existing Simulator .tpa file by changing vendor name and it still showed up under a different vendor. I renamed it to Simulator2 added some random files. On problem is that if I add a custom image the image won't show up. Only if I manually copy the image to the C:\Users\USERNAME\AppData\Roaming\TouchGFX-4.25.0\Downloads folder and rename it to thumbnail.png.
Additionally I get an error when I try generating a project with it: "Download of Simulator2 failed".
Here is my package.json file:
{
"Meta": {
"Url": "C:\\TouchGFX\\4.25.0\\app\\packages\\Simulator.zip",
"MD5sum": "EDFFB435236C401429CA7AE0898CFF3E",
"Size": 57869,
"Author": [
{
"Name": "John Doe",
"Contact": "",
"URL": ""
}
],
"LicenseUrl": "",
"Copyright": "",
"TouchGFXVersion": {
"Major": 4,
"Minor": 25,
"Build": 0
},
"CreatedAt": "2018-09-26T00:00:00Z",
"PathToDotTouchGFX": "TouchGFX",
"EmbeddedOs": "Windows"
},
"Data": {
"Version": {
"Major": 1,
"Minor": 0,
"Build": 1
},
"Name": "Simulator2",
"HumanFriendlyName": "Simulator2",
"BoardName": "PC",
"Type": "TGAT",
"Vendor": "company",
"Description": "The simulator runs exclusively on your PC without the need for any embedded target.\nUse the simulator for prototyping applications, when your hardware is not available, or for evaluating TouchGFX.\nAny display resolution and any color depth can be chosen.\nThe simulator supports a GCC and a Visual Studio™ based build.",
"DocumentationLink": "",
"Category": "",
"Images": [
"C:\\TouchGFX\\4.25.0\\app\\packages\\Simulator.png"
],
"Tags": [],
"AvailableResolutions": [
{
"Height": 600,
"Width": 1024
}],
"TargetBpp": [
16
]
}
}
If I run the package tool it overwrites my json file and changes the version. The tool does many renames by default. Such as naming files MyApplication by default. It's really confusing. There are no error messages and there are no real-world examples.
2025-07-14 7:35 AM
Hello @unsigned_char_array ,
To see the new TPA in your TouchGFX Designer, I think your TPA must be added to touchgfx\app\packages where touchgfx is your local installation.
Regards,
2025-07-14 11:04 AM
@GaetanGodart wrote:Hello @unsigned_char_array ,
To see the new TPA in your TouchGFX Designer, I think your TPA must be added to touchgfx\app\packages where touchgfx is your local installation.
Regards,
I did.
I moved it to
C:\TouchGFX\4.25.0\app\packages
But it didn't work. I didn't get any error message, so I don't know why TouchGFX is not seeing the file (I think it does see the file, but it failed to parse it or something).
2025-07-18 7:04 AM
Maybe you can help me. I tried to create a simple project, but it didn't work.
I also don't know what the "Url" parameter in the json file is for. Does it mean boards will always be uploaded? Or can you have a local board file?
2025-07-22 9:22 AM
Hello @unsigned_char_array ,
The only field that needs to be changed are the one specified in the https://support.touchgfx.com/docs/development/scenarios/scenarios-create-at . Therefore the fact that it overwrites some of your changes it's not surprising. The Url field should also be auto filed after running the first command
tgfx.exe pack -d
2025-07-23 2:18 AM - edited 2025-07-23 2:27 AM
I tried it again.
The board works.
But some things don't work.
2025-07-23 5:17 AM
Hello @unsigned_char_array ,
1- To specify the version, you can use this extra option "--version=VALUE", for instance:
tgfx.exe pack -rc --version=3.0.0 -d MyApplication_23
2- The image cannot be an image from your path unfortunately, you need to give a path from an image from internet.
3- This is not related to the packing procedure I believe. Can you open your .touchgfx and check what's in the field "Name" ?
...
"CustomContainerDefinitions": [],
"Name": "STM32N6570-DK",
"Resolution": {
"Width": 800,
"Height": 480
},
"SelectedColorDepth": 16,
...
2025-07-24 1:57 AM
@Osman SOYKURT wrote:The image cannot be an image from your path unfortunately, you need to give a path from an image from internet.
The image is hosted on a network drive mapped server. Path is something like:
"file:///K:/path_to_image/image.png"Why doesn't that work?
2025-08-04 12:09 PM
I'm unsure about if this is feasible to use a link to a mapped server. To my knowledge, only pictures hosted on internet works.
Have you tried to check the application name as I suggested in my last message btw?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.