2019-09-08 11:38 PM
I am using STM32F469 for my project. Also, I want to interface 1.54" TFT LCD with it.
I used CubeMX for pin configuration and initialisation. By default, it is initialising the graphics for 4" Touch LCD (800*480) with RGB interface.
I changed the same to 240*240 physical display size and then designed a simple GUI for test purpose using GUI Builder by STemWin.
Is this a right approach or I need t change it? Please help me out so I can start my further development.
I am attaching the CubeMX Report File for the same.
Thank You.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.