2022-03-22 11:41 AM
Hello,
If i have one "Master" project and want to use it with several touchgfx projects, what would be the best way?
So lets say i have the IDE project, Visu1 and Visu2 in GIT.
The changes of the Master IDE should be used in both TouchGFX projects.
Does anyone have an idea how to best solve this?
Thanks.
2022-03-31 2:12 AM
I just checked the Texts and Language file and it seems that the texts are all in one enum, unfortunately there is no group of texts available which would make it easy to create a list of texts based on a text group.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.