2020-10-05 11:42 AM
I'm using TouchGFX version 4.9.3
I'm able to add a modal window normally and enter the position of the background image so that it is centered. However, If I close and reopen my project to build it without selecting the modal window, then the whole modal window shows up uncentered when I run my application.
I have looked at the generated Base class for the screen. For some reason the code for setting the modal window's position is not "setXY(0,0)" but it is instead the values I entered to center the background image, for example "setXY(125,117)".
If, however, I open my project to build it after I select the modal window, then the modal window shows up centered and the generated code sets the position to 0,0.
Selecting each window in my project every time I need to make a small change in an unrelated part can waste a lot of time.
My question. Has anyone else experienced this issue? Is there any way to fix this?
Thank you
2020-10-05 9:37 PM
Hello,
Please upgrade to 4.14 (and maybe even 4.15 that will be released on October 8). If you still have the issue we will try to look at it.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.