2020-07-05 10:32 AM
Could some one help me in making SPI C-program of MAX7219, 8 digit 7 segment display using STM32F401RE
.
i have written this code in arm keil (µVision 5) it is not working, could someone help me please:
#include"stm32f4xx.h"
#include<stdio.h>
#include<string.h>
void Led_write (char data);
void delayMs(int n);
int main (void)
{
char num[] = {0x7e,0x60,0x6d,0x78,0x33,0x5b,0x5f,0x70,0x7f,0x7b};
RCC->AHB1ENR |= 0x0001;
RCC->AHB2ENR |= 0x1000;
GPIOA->MODER &= ~0xcf00;
GPIOA->MODER |= 0x8900;
GPIOA->AFR[0] &= ~0xf0f00000;
GPIOA->AFR[0] |= 0x50500000;
SPI1->CR1 = 0x031c;
SPI1->CR2 = 0x00;
SPI1->CR1 |= 0x40;
while(1)
{
for(int i=0;i<10;i++)
{
Led_write(num[i]);
delayMs(100);
}
}
}
void Led_write (char data)
{
while(!(SPI1->SR & 2));
GPIOA->BSRR = 0x00100000;
SPI1->DR = 0x0900 | data;
while(SPI1->SR & 0x80);
GPIOA->BSRR = 0x00000010;
}
void delayMs(int n)
{
for (int i=0;i<n;i++)
for (int j=0;j<3195;i++);
}
2020-07-05 4:53 PM
You need to enable SPI clock in RCC.
It's probably better to use the symbols defined in the device header, rather than numbers, for the various register bitfields values.
JW
2020-07-18 8:16 AM
hello,
I have enable the SPI1 clock in RCC using RCC->AHB2ENR |= 0x1000; using this statement.
and i have tried new code, Please help me.
/* Micro controller: STM32F401RE
PA7 DIN
PA5 SCK
PA4 SS
driver MAX7219: 8 digit 7 segment display */
#include"stm32f4xx.h"
#include<stdio.h>
void init_SPI1 (void); // initialization of SPI1
void write_SPI1 (uint16_t data); // writing data to SPI1
void delayMs (uint16_t n); // generating delay
uint16_t shut_Addr = 0x0c00; //Normal operation
uint16_t norm_Addr = 0x0c01; //Normal operation
uint16_t intn_Addr = 0x0a05; //intensity register
//uint16_t code_Addr = 0x0900; //address of decode mode
uint16_t dig1_Addr = 0x0100; //selecting digit 1
int main (void)
{
init_SPI1();
write_SPI1(norm_Addr);
write_SPI1(intn_Addr); // for intensity: intensity is 0x0e
while(1)
{
write_SPI1 (dig1_Addr | 0x01); // for DIGIT1: sending value 3
}
}
void write_SPI1 (uint16_t data) //writing something to MAX7219
{
while(!(SPI1->SR & 0x02)); //wait until transfer buffer empty
GPIOA->BSRR = 0x00100000; //Slave select = 0
SPI1->DR = data;
while(SPI1->SR & 0x80); //wait for transmission done
GPIOA->BSRR = 0x00000010; //Slave select = 1
}
void init_SPI1(void) //initializing the MAX7219
{
RCC->AHB1ENR |= 0x0001; //Enabling clock of GPIOA
RCC->APB2ENR |= 0x1000; //Enabling clock of SPI1
GPIOA->MODER &= ~0xcf00; //resetting PA5, PA7: Alternate function and PA4: output function
GPIOA->MODER |= 0x8900; //set PA5, PA7: Alternate function and PA4: output function
GPIOA->AFR[0] &= ~0xf0f00000;
GPIOA->AFR[0] |= 0x50500000; //set PA5, PA7: Alternate function
SPI1->CR1 = 0x0b14; //seting baudrate, 16 bit format
SPI1->CR2 = 0x0000;
SPI1->CR1 |= 0x0040; //Enabling SPI1
}
void delayMs(uint16_t n) //generting of delay in n ms
{
for (int i=0; i<n; i++)
for (int j=0; j<3195; i++);
}
2020-07-18 8:18 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.