2018-06-07 5:24 PM
I'm trying to do double buffering using the hardware, STMF32492I.. so first I'm initalizing two layers in two different addresses.
Then I write to the back buffer, switch the back buffer..
But The problem I get multiple copies of the sprite that is animated, so its either I'm drawing to the front buffer multiple times, or the back buffer needs to be cleared.
Here is how I'm doing it
void main{ while (1)
{ LTDC_switch_framebuffer(); // draw spries }}void LTDC_switch_framebuffer(void){ LTDC->SRCR = LTDC_SRCR_VBR; // reload shadow registers on vertical blank while ((LTDC->CDSR & LTDC_CDSR_VSYNCS) == 0); // wait for reload ; flip ^= 1; BSP_LCD_SetLayerVisible(flip, ENABLE); BSP_LCD_SelectLayer(1-flip); }#ltdc #double-buffer #stm32f4-ltdcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.