2021-08-01 11:21 PM
STM32F746G_DISCO by default has 480 x 272 . We changed the display to 800 x 480 (EK9716B LCD and FT7311 Touch controller) .
Then we used the TouchGFX 4.17 / 4.16 to generate the code and updated the parameters to reflect 800 x 480.
The 800x480 images are displayed properly on the LCD.
When we touch the screen at any pixel beyond 480, we can see that STM32TouchController::sampleTouch (x, y) does indeed detect touch.
However the user code in flexButtonCallbackHandler ( ) is not getting called by TouchGFX framework
The same code works well for Simulator.
The lower lever I2C Touch controller driver detects the touch and during debug with disco-board, shows the correct coordinates.
Did anyone face a similar problem ? Why do you think, TouchGFX framework is not calling the user code for a pixel > 480 ?
2021-08-02 10:01 PM
@Martin KJELDSEN Can you please look into above query and let us know if you have any pointers for debugging the same.
2021-08-09 5:11 AM
Hi - Just got back from vacation.
If touch is detected but a certain widget is not receiving touch, please verify that the coordinates read are actually where the widget is located.
2024-10-22 9:58 PM
Can you please tell me how you interacted with the touch panel? I am also using the same New Haven display (EK9716B LCD and FT7311 Touch controller) for my application. I have used 4.7K pullup on SDA and SCL lines. I am able to read/write FT7311 registers but cannot get the correct touch points. I am also able to detect the number of touchpoints correctly. Can you please provide any reference on how you implemented your touch functions for FT7311?
I have attached the display datasheet.
Thank You.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.