2020-01-01 7:15 AM
Hello,
So i did try to port my project to the STM32H747I-DISCO board, to evaluate if possible
to switch to the new dual core H7 chip.
It seems that the DSI driver implements some anti tearing feature, that splits the screen into zones, that subsequently allocate the layer buffers to each zone.
Also it seems now is expected that emWin functions to switch layers via GUI_Delay() call that has to be placed, in the GUI task. Without this call just default layer (part of screen) is visible.
This is significant change to the way layers were used in older ST examples (for F7 and H7).
Has this change been explained somewhere in some Application Note, that i have maybe missed ?
Also it seems the LCD driver uses basic 565 and 4444 driver from emWin, instead the full
8888 version with alpha. Is this limitation of the DSI hardware (cheap LCD) or to make
the STemWin match the Embedded Wizard demo ? And speaking about the latter, why only binary ?
Thank you!
K.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.