2020-01-01 12:54 AM
I stored all image content from section ExtFlashSection on my sd card, when loading:
#define CACHE_SIZE 3000000
void touchgfx_init()
{
uint16_t dispWidth = 800;
uint16_t dispHeight = 480;
uint16_t *cache = (uint16_t*)malloc(CACHE_SIZE);
HAL& hal = touchgfx_generic_init<STM32H7HAL>(dma, display, tc, dispWidth, dispHeight,
cache, CACHE_SIZE, 1000);
Bitmap::cacheAll();
...
}
the program crashes in cacheAll() before calling my overwritten blockCopy().
Is there a demo for Bitmap::cacheAll()?
2020-01-01 1:29 AM
After I checked code, I found that,
In BitmapDatabase.c, bitmap_database[] stores the static bitmap pointers like "_blue_buttons_round_edge_small".
and "_blue_buttons_round_edge_small" has been put into my sd card by me. So dynamic loading image is impossible as describled in touchgfx knowledge base Non-memory mapped external flash.
I am use touchgfx 4.12.3, the document in knowledge is not updated?
2020-01-01 5:27 AM
It runs ok after I changed address from 0x09000000 to 0x24000000 as document suggested.
however I think, cacheAll() should not access these fake address, the address 0x09000000 will cause hardfault on st mcu.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.