2017-08-29 3:09 AM
I have an array of luminance representing a picture in grayscale. Data are captured using DCMI. I need to compress these data using JPEG unit available in F7 series, but I can't find any application note describing JPEG unit, and also I don't know what functions I need to use to acheive this requirement.
Can anybody provide me a simple example?
#jpeg #stm32Solved! Go to Solution.
2017-08-29 8:35 AM
I suspect the JPEG unit uses third-party IP, so don't expect super detailed docs on the internal mechanics. Expect just a couple of buffers, and shoveling data in/out, and a streaming paradigm.
I do remember seeing a whole slew of examples under the HAL/Cube install,
sweden
has identified a bunch above, but suspect there are also examples for the DISCO boards which are likely to be far more accessible.2017-08-29 4:00 AM
1. Find where is located your STM32CubeMX repository by opening 'Help -> Updater settings...'
2.
Go to STM32Cube_FW_F7_V1.7.0/Projects/STM32756G_EVAL/Applications/LibJPEG in your repository to find encoder and decoder example projects
Edit:
It turns out the project above doesn't use the hardware module, but there are other examples which do:
STM32Cube_FW_F7_V1.7.0/Projects/STM32F769I-Discovery/Examples/JPEG/JPEG_DecodingUsingFs_DMASTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_DecodingFromFLASH_DMASTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_DecodingUsingFs_DMASTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_DecodingUsingFs_InterruptSTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_EncodingFromFLASH_DMASTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_EncodingUsingFs_DMASTM32Cube_FW_F7_V1.7.0/Projects/STM32F769I_EVAL/Examples/JPEG/JPEG_MJPEG_VideoDecoding2017-08-29 8:35 AM
I suspect the JPEG unit uses third-party IP, so don't expect super detailed docs on the internal mechanics. Expect just a couple of buffers, and shoveling data in/out, and a streaming paradigm.
I do remember seeing a whole slew of examples under the HAL/Cube install,
sweden
has identified a bunch above, but suspect there are also examples for the DISCO boards which are likely to be far more accessible.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.