2019-12-05 12:44 AM
Hi all,
I`m trying to decode jpg with JPEG Codec, and I reference the sample code from CubMX Official code { JPEG_DecodingUsingFs_DMA }, then inserted to my code.
And now it stocks in this function:
do
{
JpegProcessing_End = JPEG_OutputHandler(&JPEG_Handle);
}while(JpegProcessing_End == 0);I have checked the SDRAM & HAL_JPEG_MSP setting, and nothing wrong .
By the way, it`s a little similar from :https://community.st.com/s/question/0D50X0000BBqYgrSQF/jpeg-codec-decoding-does-not-endcomplete
, but I use this { JPEG_DecodingUsingFs_DMA } project with SDMMC.
Can anyone help with this?
Thanks!
2019-12-05 11:11 PM
Hi,
I find some problem, if there are someone can help,please remain your suggestions!
Just like what I post on topic, the function { JPEG_OutputHandler } in down below.
When it goes in this function, it always get Jpeg_HWDecodingEnd = 0 , so it will keep doing the do..while function never ending.
uint32_t JPEG_InputHandler(JPEG_HandleTypeDef *hjpeg)
{
if(Jpeg_HWDecodingEnd == 0)
{
if(Jpeg_IN_BufferTab[JPEG_IN_Write_BufferIndex].State == JPEG_BUFFER_EMPTY)
{
if(f_read (pFile, Jpeg_IN_BufferTab[JPEG_IN_Write_BufferIndex].DataBuffer , CHUNK_SIZE_IN, (UINT*)(&Jpeg_IN_BufferTab[JPEG_IN_Write_BufferIndex].DataBufferSize)) == FR_OK)
{
Jpeg_IN_BufferTab[JPEG_IN_Write_BufferIndex].State = JPEG_BUFFER_FULL;
}
else
{
Error_Handler();
}
if((Input_Is_Paused == 1) && (JPEG_IN_Write_BufferIndex == JPEG_IN_Read_BufferIndex))
{
Input_Is_Paused = 0;
HAL_JPEG_ConfigInputBuffer(hjpeg,Jpeg_IN_BufferTab[JPEG_IN_Read_BufferIndex].DataBuffer, Jpeg_IN_BufferTab[JPEG_IN_Read_BufferIndex].DataBufferSize);
HAL_JPEG_Resume(hjpeg, JPEG_PAUSE_RESUME_INPUT);
}
JPEG_IN_Write_BufferIndex++;
if(JPEG_IN_Write_BufferIndex >= NB_INPUT_DATA_BUFFERS)
{
JPEG_IN_Write_BufferIndex = 0;
}
}
return 0;
}
else
{
return 1;
}
}Then I check detail of the project, it can leave this function by :
void HAL_JPEG_DecodeCpltCallback(JPEG_HandleTypeDef *hjpeg)
{
Jpeg_HWDecodingEnd = 1;
}But it`s something strange, I search HAL_JPEG_DecodeCpltCallback which is called by HAL_JPEG_Init ,there are called by other too but this most associate.
And HAL_JPEG_Init didn`t open that, so how should us use it?
If USE_HAL_JPEG_REGISTER_CALLBACKS == 1 is true, then HAL_JPEG_MspInit won`t be executed and it is wrong method for this project.
#if (USE_HAL_JPEG_REGISTER_CALLBACKS == 1) --> It didn`t open
if (hjpeg->State == HAL_JPEG_STATE_RESET)
{
/* Allocate lock resource and initialize it */
hjpeg->Lock = HAL_UNLOCKED;
hjpeg->InfoReadyCallback = HAL_JPEG_InfoReadyCallback; /* Legacy weak InfoReadyCallback */
hjpeg->EncodeCpltCallback = HAL_JPEG_EncodeCpltCallback; /* Legacy weak EncodeCpltCallback */
hjpeg->DecodeCpltCallback = HAL_JPEG_DecodeCpltCallback; /* Legacy weak DecodeCpltCallback */
hjpeg->ErrorCallback = HAL_JPEG_ErrorCallback; /* Legacy weak ErrorCallback */
hjpeg->GetDataCallback = HAL_JPEG_GetDataCallback; /* Legacy weak GetDataCallback */
hjpeg->DataReadyCallback = HAL_JPEG_DataReadyCallback; /* Legacy weak DataReadyCallback */
if (hjpeg->MspInitCallback == NULL)
{
hjpeg->MspInitCallback = HAL_JPEG_MspInit; /* Legacy weak MspInit */
}
/* Init the low level hardware */
hjpeg->MspInitCallback(hjpeg);
}
#else
if (hjpeg->State == HAL_JPEG_STATE_RESET)
{
/* Allocate lock resource and initialize it */
hjpeg->Lock = HAL_UNLOCKED;
/* Init the low level hardware : GPIO, CLOCK */
HAL_JPEG_MspInit(hjpeg);
}
#endif /* USE_HAL_JPEG_REGISTER_CALLBACKS */
It is what I want to share my question, and I`ll keep research it.
Hope someone can really help!
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.