2020-12-10 9:56 AM
I have installed the example software for the STM32L476VG microcontrooller for the audio recorder.The HAL driver files for the LCD screen has been installed also.The LCD screen wont enable.Is there a soldered connection on the bottom of the PCB board or something that can be done to get the display to operate?
2020-12-10 10:14 AM
The STM32L476G-DISCO?
Not a board I have to hand, but seem to recollect the demo working out of the box?
The schematic/user manual should enumerate the solder bridges, and the README files frequently call out specific requirements/expectations.
Try the example, uses the display at some point, and measures current, etc.
STM32Cube_FW_L4_V1.14.0\Projects\32L476GDISCOVERY\Examples\BSP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.