2021-02-26 5:50 AM
I need image progress width background 500, but indicator slim 15px .
Exist an library way or i need write full new class?
I see now only one way create big transparent indicator image, that waste space and slow render.
/**
* @fn virtual void ImageProgress::setBitmap(touchgfx::BitmapId bitmapId);
*
* @brief Sets the bitmap id.
*
* Sets the bitmap id to use for progress. Please note that the bitmap is tiled
* which will allow smaller bitmaps to repeat and save memory.
*
* @param bitmapId The bitmap id.
*
* @see getBitmap
* @see TiledImage
*/
virtual void setBitmap(touchgfx::BitmapId bitmapId);
2021-03-01 1:30 AM
Hi,
Could you provide more detail on what you are trying to do ? I am not sure I understand properly what you mean by "indicator slim 15px" for example.
You can set the widgth/height of the progress indicator in the "Progress Position" section in the widget settings in TouchGFX Designer. I was able to set it to an imageProgress widget both the background and the progress indicator images with 500x500 images. I had no issues with the progress indicator image being cut by 15px (that is what i understand from your message).
Could you also share a screenshot of your issue or provide the images you want to use ?
/Romain
2021-03-01 4:22 AM
I need horizonatal gauge with vertical indicator - not angled. as IMAGE
Background size 500x75 indicator size 15x70
Now i can only use indocator 470x70 transparent nothing...
2021-03-03 3:24 AM
@Romain DIELEMAN no idea?
2021-03-03 5:30 AM
Hi,
I was not able to replicate your issue, could you share the images you are using ?
/Romain
2021-03-03 7:25 AM
Ahh i dont have issue, i have space issue :
For example as i write my background is 500x75 RGB888 = 109kB in flash
When i use imageProgress i need too indicator image 470x70 winth alpha without L8 coding next 128kB
my app dont have one imageProgress and screen dont refresh only this.
When i continue calculating for animate one indicator 470x70 in 50Hz screen sw generates write memory bandwidth 5MB/s
L8 reduce flash to 1/3 , but framebuffer memory band isnt changed and calculate part is next stage.
Indicator image:
......................................................................................................................................|here is end image
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.