2019-12-23 10:26 PM
Hello
In the case of F746-DISCO, the resolution is 480 × 272,
For example, how to customize when connecting 800x600 LCD?
Thank you.
2019-12-25 4:46 AM
TouchGFX derives the screen resolution from the LTDC interface setup. if you change it there it should change for the TouchGFX as well.
2019-12-25 2:51 PM
Hello HP's
OK.
Thank you for your response.
2019-12-31 10:12 AM
Did this work? I will be doing a similar change soon.
I presume the LCD's ribbons are soldered to the Disco board (I have not looked). Did you install a connector?
Bob
2020-01-02 12:44 AM
There's no connector under the screen - it's soldered directly on the board. I've looked. Also, the connector is really wide, like 1mm pitch or similar, so soldering on a connector is not trivial.
2020-01-03 4:22 PM
Not tried yet.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.