2020-04-03 12:17 AM
Thank you for helping.
environment
STM32CubeIDE Ver1.3.0
STM32CubeMX Ver5.5.0
TouchGFX Ver4.12.3
Board: STM32F769I-DISCO
This board is connected to LCD by DSI interface.
How do I change the source code to make the interface RGB parallel when creating a custom board?
If I remove MX_DSIHOST_DSI_Init () and set GPIO to output in RGB parallel, do I need any other changes?
Thank you.
2020-04-03 1:24 AM
Generally, you can check the STM32F746G-DISCO or other ATs that have an LTDC. Can we start there? I think you'll see what to do (LTDC interrupt handler signals OSWrapper::signalVSync to unblock TouchGFX Engine), so it's a lot simpler.
2020-04-03 5:55 PM
Dear Martin,
Thank you for helping.
It is assumed that the device uses F769.
What should I think?
2020-04-30 3:39 AM
Did you take a look at the code in the application templates e.g. F746G-DISCO? Generally, if you remove the DSI HOST configuration in CubeMX and tell TouchGFX Generator to do Parallel RGB (LTDC) then you will have the appropriate driver. Should be all you need.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.