2022-10-04 8:07 PM
2022-10-05 3:18 AM
Hi @Community member and welcome to the Community :),
If you used the STM32F413H_Discovery_REVE board, please make sure to select the target board revision in the project options as mentioned in the stm32f413h_discovery.h.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-05 8:50 PM
Hi @KDJEM.1 / Kaouthar,
Thank you for your reply.
I used STM32F413H-DISCO MB1274-F413ZHT6-E03.
I tried defined flag USE_STM32F413H_DISCOVERY_REVE in line 87 in the stm32f413h_discovery.h file but result shows same error.
Is there any other possible solution?
Thanks again.
2022-10-12 6:09 AM
Hi @Community member,
I confirm the issue: the STM32F413H-DISCO-REVE03 is not supported for BSP example.
In fact, the FRD154BP2902-D-CTQ LCD should use the BSP component ft3x67.
I reported this issue internally.
Internal ticket number: 136410 (This is an internal tracking number and is not accessible or usable by customers).
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-13 7:39 PM
Hi @KDJEM.1 ,
Is there any other example project that I can use to calibrate and test my touch panel for STM32F413H-DISCO-REVE03 board? or any example project with minor modification?
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.