2022-06-21 4:54 PM
hello
I inquire about TouchGFX Compile error.
To call a specific function by including discovery.h in Model.cpp
A compile error occurs.
However, in CubeIDE, it compiles normally and runs well.
I want to know why a compile error occurs in TouchGFX and a normal compile in CubeIDE.
1.The development environment is as follows
2. The source of model.cpp is as follows.
===================================================================
#ifndef SIMULATOR
extern "C" {
#include "stm32H7xx.h"
#include "stm32h735g_discovery.h"
}
#endif
void Model::tick()
{
#ifndef SIMULATOR
int button_sample = BSP_PB_GetState(BUTTONn); //BUTTONn // BUTTON_USER
if (button_sample != 0x000F)
{
if( buttonState != button_sample )
{
modelListener->PUI_data(button_sample);
buttonState = button_sample;
}
}
else
{
buttonState = button_sample;
}
}
===================================================================
3.The error message in TouchGFX is as follows.
===================================================================
Compile
make -f ../gcc/Makefile -j8
Reading TouchGFX/application.config
Compiling TouchGFX/gui/src/scrtopcook_screen/ScrTopCookView.cpp
Compiling TouchGFX/gui/src/scrtopcook_screen/ScrTopCookPresenter.cpp
Compiling TouchGFX/generated/gui_generated/src/scrbottom_screen/ScrBottomViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrtopcook_screen/ScrTopCookViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrtopset_screen/ScrTopSetViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrauto_screen/ScrAutoViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrmain_screen/ScrMainViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrtop_screen/ScrTopViewBase.cpp
Compiling TouchGFX/generated/gui_generated/src/scrloading_screen/ScrLoadingViewBase.cpp
Compiling TouchGFX/generated/images/src/image_Pause.cpp
Compiling TouchGFX/generated/images/src/BitmapDatabase.cpp
Compiling TouchGFX/generated/images/src/image_restart.cpp
Compiling TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp
Compiling TouchGFX/target/generated/TouchGFXConfiguration.cpp
Linking TouchGFX/build/bin/target.elf
TouchGFX/build/STM32H735G-DK/TouchGFX/gui/src/model/Model.o: In function `Model::tick()':
c:\TouchGFXProjects\Noble_cooker/TouchGFX/gui/src/model/Model.cpp:29: undefined reference to `BSP_PB_GetState'
collect2.exe: error: ld returned 1 exit status
gcc/Makefile:293: recipe for target 'TouchGFX/build/bin/target.elf' failed
make[2]: *** [TouchGFX/build/bin/target.elf] Error 1
gcc/Makefile:289: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
../gcc/Makefile:49: recipe for target 'all' failed
make: *** [all] Error 2
===================================================================
2022-06-21 9:50 PM
TouchGFX use different makefile as CUBE. You need add search path to added headers and add source files into TGFX makefile.
2022-06-21 10:10 PM
thank you for your reply.
I don't know how to modify the makefile in TouchGFX.
Are there any guides provided?
2022-06-22 1:40 AM
@MM..1 but the posted error is not about problems finding a header file?
2022-06-22 1:47 AM
@mSH.1 "To call a specific function by including discovery.h in Model.cpp A compile error occurs. However, in CubeIDE, it compiles normally and runs well."
So the TouchGFX build is C++ - is the CubeIDE build also C++, or just plain C ?
This doesn't look right:
#ifndef SIMULATOR
extern "C" {
#include "stm32H7xx.h"
#include "stm32h735g_discovery.h"
}
#endifDid you mean:
#ifdef __cplusplus
extern "C"
{
#endif
#include "stm32H7xx.h"
#include "stm32h735g_discovery.h"
#ifdef __cplusplus
}
#endif@mSH.1
2022-06-22 2:29 AM
hello @Andrew Neil
Thanks for the useful feature.
As I was informed, the moel.cpp part was modified as follows.
#ifdef __cplusplus
extern "C"
{
#endif
#include "stm32H7xx.h"
#include "stm32h735g_discovery.h"
#ifdef __cplusplus
}
#endif
But the same error occurs.
It occurs only in touchGFX and compiles normally in CubeIDE.
The error message in TouchGFX is as follows.
Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.project files generated inside project folder
This is STM32CubeIDE project updater: Working on ../STM32CubeIDE/.project
.cproject file: ../STM32CubeIDE/.cproject
Float ABI: hard
Writing STM32CubeIDE project file: ../STM32CubeIDE/.project
Writing STM32CubeIDE project file: ../STM32CubeIDE/.cproject
Done
Compile
make -f simulator/gcc/Makefile -j8
Reading ./application.config
Compiling gui/src/scrbottom_screen/ScrBottomView.cpp
Compiling gui/src/scrbottom_screen/ScrBottomPresenter.cpp
Compiling gui/src/scrtopcook_screen/ScrTopCookView.cpp
Compiling gui/src/scrtopcook_screen/ScrTopCookPresenter.cpp
Compiling gui/src/containers/CustomContainer_temp_wheel.cpp
Compiling gui/src/scrtopset_screen/ScrTopSetPresenter.cpp
Compiling gui/src/scrtopset_screen/ScrTopSetView.cpp
Compiling gui/src/model/Model.cpp
gui/src/model/Model.cpp:18:10: fatal error: stm32H7xx.h: No such file or directory
#include "stm32H7xx.h"
^~~~~~~~~~~~~
compilation terminated.
generated/simulator/gcc/Makefile:196: recipe for target 'build/MINGW32_NT-6.2/gui/src/model/Model.o' failed
make[2]: *** [build/MINGW32_NT-6.2/gui/src/model/Model.o] Error 1
make[2]: *** Waiting for unfinished jobs....
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Failed
2022-06-22 2:59 AM
@mSH.1 "As I was informed, the moel.cpp part was modified as follows"
I don't know the context of that snippet, so don't know if it's actually what you wanted - but certainly the original didn't look right.
There may be other places in your code with similar issues?
Do you understand the issues of mixing C and C++, and why/when the extern "C" is required?
You are now getting errors due to not finding header files - so, as @MM..1 said, you do need to adjust your include paths...
2022-06-22 7:17 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.