2020-10-19 12:36 PM
There is no application template for H745. How can i adapt something to make it a fast run?
Trying for almost one week now. I am out of ideas.
Please help
2020-10-19 3:09 PM
No need to make three threads for the same issue. The problem seems to be you've erased the flash on the ST-Link chip, but you haven't answered questions in the other threads you've opened.
https://community.st.com/s/question/0D53W00000LFNK5SAP/h750-discovery-board-stlink-v3
2020-10-19 3:36 PM
Which STM32H745 board? The DISCO or the NUCLEO?
Not sure they have a Dual Core H7 build for TouchGFX yet, but they have talked about it. Perhaps there is a beta available.
Otherwise look at the Application/Demonstrations provided for the board under the CubeH7 example trees
2020-10-20 12:01 AM
The disco board. There is a demo for H750. Is there any tutorial for creating a Application Template for TouchGfx?
2020-10-21 8:08 AM
Hello @BHure.1 ,
There’s an application template for STM32H750B-DK within STM32CubeH7 MCU package, provides a reference UI template (examples) that can be used to build any firmware application: STM32Cube_FW_H7_V1.8.0\Projects\STM32H750B-DK\Templates\Template_Project
You can refer to the TouchGFX User guide, TouchGFX User manual and TouchGFX MOOC, this will help you to create your STM32 based application using TouchGFX.
Have a look also on the TouchGFX demo and get inspired from them: STM32Cube_FW_H7_V1.8.0\Projects\STM32H750B-DK\Demonstrations\TouchGFX
I hope that this is useful for you.
Imen
2020-10-21 10:45 AM
Hello Imen,
The demo is for H750. I have H745. If i try to flash it on the board, i get a blank display.
How can i adapt the example for H745 ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.